STM32 MCUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New possibilities for the ultra-low power segment!

STM32U0 is the first Cortex-M0+ with a static consumption of only 160 nA in standby mode with RTC (Real-Time Clock) and 16 nA in shutdown. It also achieves 118 points in CoreMark and targets SESIP level 3 and PSA level 1 focusing on firmware code pro...

gif-stm32u0.gif

100ns trigger pulses

Hello team, which of the STM32 microcontroller is able to generate single trigger pulses in steps of 100ns +/- 10ns? Best regards,Jochen

JR1 by Associate II
  • 8 Views
  • 0 replies
  • 0 kudos

A question on pin labeling for STM32H7

The STM32H7 reference manual (stm32h723zg.pdf) contains several tables describing he pin mappings (pin to functions).In Table 7 and 8, for pin A0, A5, and A15, it lists the pin function as "TIM2_CH1/TIM2_ETR" for alternate function #0. Should this be...

sidney by Associate II
  • 20 Views
  • 0 replies
  • 0 kudos

empty SD card sensor tile probox

good morning. i am actually trying to load on my an sd card my data of the sensor tile.box. Unfortunately, I only get blank tables with only the top written. I uploaded a configuration to make it and then uploaded as seen on those photos. am I missin...

Jad_0-1726993052664.png Jad_1-1726993077075.png Jad_2-1726993122799.png
Jad by Associate II
  • 25 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G030 is support I2C master?

Have an issue with connection I2C sensor to STM32G030 chip.  Function HAL_I2C_IsDeviceReady alvais return HAL_ERROR.  Looks like this controller are not support I2C master, but documentation said: Features of the I2C peripheral: I2C-bus specification...

Bigdan by Visitor
  • 133 Views
  • 6 replies
  • 2 kudos

Resolved! STM32F103C8 SysTick initialisation issue

Hi,I am using STM32F103C8T6 Blue pill board, STM32 CubeIDE 1.16.0, Build: 21983_20240628_1741 (UTC) on Ubuntu 22.04.5 LTS and ST Link v2 debugger. I am able to upload code, execute it and debug it via SWD.I am using CubeIDE's Pinout & configuration u...

akosbalogh01_0-1726951418169.png

EEPROM

I am in work with a product firmware with STM32G030k8 with additional EEPROM M24C04 I coudlnt ble to instal the driver files .Is this the righ tway am doing,can any one please address this?I am not able to hightlight or install Thanks.

meena_0-1726984378397.png
meena by Associate III
  • 35 Views
  • 0 replies
  • 0 kudos

External interupt

Hi all, I currently work on STM32F030K6 .I am working with a reed switch connected to pin PA8 (EXTI8).I havec onfigured the PIN like : "external Interrupt Mode rising/falling ....I need to perform an action on the rising edge AND on the falling edge....

JJoao.1 by Associate II
  • 62 Views
  • 1 replies
  • 0 kudos
Labels