STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Log Data externally with STM32F767ZI and Simulink

Hey everyone,I want to use a STM32F767ZI to develop driving safety functions for electric scooters.The functions and Code are developed on Simulink using the Support Package for nucleo boards. I would like to log data from the MCU directly to a SD-Ca...

LKlau.1 by Associate
  • 670 Views
  • 3 replies
  • 1 kudos

STM32F407VGT6U (DISC1) External mode : Could not connect to target application: XCP internal error: timeout expired, in response to XCP CONNECT command

Hello guys!I'm trying to use external mode with STM32F407VGT6U(older version of this discovery board) and Embedded Coder Support Package for STMicroelectronics STM32 Processors, I'm running on Matlab r2023a with all the support packages freshly insta...

GDan.2 by Associate
  • 737 Views
  • 0 replies
  • 2 kudos

How to enable UART with STM32F413 via MATLAB Simulink?

Hi guys,I'm working on UART with STM32F413 via MATLAB Simulink recently.I've followed this tutorial: 《Getting Started with STMicroelectronics STM32 Processor Based Boards》 from MathWorks.And I can already turn on LED via MATLAB Simulink. And next ste...

0693W00000aH27vQAC.png
YFu.1 by Associate
  • 516 Views
  • 0 replies
  • 1 kudos

STM32F4 USART_Receive block usage problem in Simulink

Hi everyone,I am trying to read a laser sensor through UART of STM32F4 inside Simulink. The laser sensor's refresh rate is 10 Hz approximately but it does not give the data periodically. I am using UART Interrupt for reading action. There are two cas...

Hi, set stm32H750 tim, Error in 'deviceManage/Function-Call Subsystem/Timers': Initialization commands cannot be evaluated. TIMERS_Config function : Can not find which APB timer TIM1 is connected to.Default preference value STM32TIMAPB set to APB1 is use

Hi, set  stm32H750 tim, Error in 'deviceManage/Function-Call Subsystem/Timers': Initialization commands cannot be evaluated. TIMERS_Config function : Can not find which APB timer TIM1 is connected to.Default preference value STM32TIMAPB set to APB1 i...

0690X00000D8vuiQAB.png
lling.1 by Associate II
  • 1182 Views
  • 15 replies
  • 0 kudos

External Mode with STM32L476RG not working

Hi all.I'm trying to run external mode simulation using:Matlab R2022a.CubeMx 6.2.0STM32 Mat\Target(not sure which version) Nucleo L476RGI have created a simple LED example to test the external mode and I used the Embedded Coder to integrate it with t...

0693W00000QKg6AQAT.png
MArvi.1 by Associate II
  • 287 Views
  • 1 replies
  • 0 kudos
Labels