STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1713 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4868 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9539 Views
  • 5 replies
  • 3 kudos

CSConnect Errors When Generating Custom Project

Hello,I am working on a custom FOC Inverter Board.  I am trying to assign the pins for current sensing, but I keep getting warnings.  I am using an STM32G431CBT6 MCU, and I completed all the other pin assignments without issue.  Here is the Current S...

reesed13_0-1779544074338.png

Motor control with resolver

Good afternoon,I am working with the STSW-TTM005 example for a resolver-equipped motor and encountered an issue:Link: STSW-TTM005 | Product - STMicroelectronicsThe motor does not rotate, but instead oscillates between windings.In sensorless mode, the...

P-NUCLEO-IHM03 giving driver protection fault

Good evening, I am trying to use a P-NUCLEO-IHM03 pack.I have generated the project using the X-CUBE-MCSDK version 6.4.2 and STM32cubeMX version 6.17.0, built and flashed the project on the board. The problem is that as soon as I try to start the mot...

giulioTam_0-1779283331625.png giulioTam_1-1779283649343.png Screenshot 2026-05-20 152342.png giulioTam_2-1779283920065.jpeg

MotorControl Workbench parameters explanation

Hi everyone, I’m using MotorControl Workbench with X-NUCLEO-IHM08M1 and NUCLEO-G474RE and browsing through the user manual: file:///C:/Program%20Files%20(x86)/STMicroelectronics/MC_SDK_6.4.2/Documentation/html/pages.htmlIn my project (under the vario...

luke514_0-1778593160139.png luke514_1-1778593588082.png
luke514 by Senior
  • 101 Views
  • 2 replies
  • 1 kudos

MCSDK compilation error

hi, I created a project by the MCSDK, i tried running it as a C++ project, but im getting an error compilation that i cant solve:   ../../MCSDK_v6.4.2-Full/MotorControl/MCSDK/MCLib/Any/Inc/revup_ctrl.h: In function 'void RUC_Stop(RevUpCtrl_Handle_t...

Ofer by Senior
  • 219 Views
  • 10 replies
  • 4 kudos