STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CHOOSE MCU

Hi.I work on BMS. I want a master-slave topology. I want to use 300 slave cards and 1 master card. This BMS is for automotive. I check ST MCU. I guess, The card should be 10-bit I2C. Because I want 300 Slave cards. So, Can you Help me this subject? W...

bngstskn by Associate II
  • 265 Views
  • 9 replies
  • 7 kudos

Broken Open Drain

Hi,I have a defect on the I2C on a STM32L151CBU6A SDA Pin (PB9). Every external component beside a 4.7k pullup resistor has been removed.The system is running on 3.6 V and if I just let the pin toggle in Push/Pull configuration I am getting a clean 3...

v_g by Associate
  • 399 Views
  • 3 replies
  • 0 kudos

I2C error recovery

Posted on August 24, 2013 at 12:05Hello,I'm trying to make the STM32L152  I2C communication failure-proof against glitches/short-circuits. There's an API command I2C_SoftwareResetCmd which seems to be the cure, but i can't find any proper example or...

Problem calibrating MSI clock using LSE

Hello, I've been trying to calibrate the system clock of a Nucleo-64 board (STM32l152) using approach proposed in AN3300 to compensate the temperature error. The proposed solution works fine with HSI clock running at 32MHz. At room temperature the op...

VMoro.3 by Associate
  • 159 Views
  • 2 replies
  • 0 kudos

flash write in stm32H743iit6

hi there,I have a stm32H743iit6 and I wish to write a uint32_t array in it flash. I use sector 6 to 7 of Bank1 to write my array to. first I fill my array with number of 0 to 69 like so for (int i = 0; i < 70; i++)//10 { flash_buffer_W[i]=i; }  a...

Ala by Senior
  • 201 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L100RC temperature sensor

Does the STM32L100RC have a temperature sensor?RM0038 refers to the temperature sensor in the STM32L1 line of processors. However, the STM32L100RC datasheet only mentions "tempsensor" in table 4 and nothing else anywhere. CubeIDE will allow the tempe...

km by Associate
  • 250 Views
  • 3 replies
  • 1 kudos

STM32L151VE ADC

"The ADC of STM32L151VE is not functioning properly. The output values of the ADC appear to be random. Does anyone know how to resolve this issue?

20230627145511809.jpg
Labels