Help needed to understand the circuits of the x-nucleo-ihm08m1
Hi, is there anyone who can help me to understand the circuits of the x-nucleo-ihm08m1 ? Like explaining to me how the figure 5 does the analog conditiong and current protection.
Hi, is there anyone who can help me to understand the circuits of the x-nucleo-ihm08m1 ? Like explaining to me how the figure 5 does the analog conditiong and current protection.
Can't post screenshots.RM0401 rev3 ('F410), RCC_APB2ENR contains EXTIEN. There is no such bit in any other STM32, EXTI is unconditionally enabled everywhere else. There is no respective reset bit in RCC_APB2RSTR. Is this bit real?in the same RM0401 r...
It should be FLITF.It's also in the 3rd figure on the next page.The typo is also in RM0364, but it's corrected in RM0313.Can't these figures be redrawn so that masters are on top, and slaves on right, as is in other 'Fx RMs?JW
Hi,while doing a symbol for the Nucleo in KiCad I found that the Pin CN7.14 should be PA7 instead PB5.The sub-note (3) is correct.Best regardsMarco
[This is a reconstruction of a thread I've started on Apr 7, 2017, but got lost in the two forum software transitions since then.]In STM32F40x and STM32F41x Errata sheet DocID022183 Rev 8, 2.1.13 Delay after an RCC peripheral clock enabling, there ...
UART transmitter transmits wrong ascii value to my pc. what is the problem in my code..??I put a charecter in Data Register, but serial terminal show another ascii code.My IDE is KeiluVision5. the code is in below..... #include<stdint.h>#include<std...
Hello Community,I am working on a Vibration Measurement system that will be subjected to lifetime vibrations ranging from 10Hz to 2000Hz at approximately 1g with expected lifetime of 2 years with 16 hours daily vibration & 8 hours of no vibration.I'm...
Hi, everyone. I am using stm32l496 and I my application requires me to keep all data in ram after reset. Now i followed these instructions in this link. https://interrupt.memfault.com/blog/noinit-memory it works, like I expected but the thing is I wa...
I've noticed that the frequencies written in the reference manual are different from the ones used in the HAL.Is there a good reason they are different? Which ones are correct?I attached a screenshot from page 407 of the reference manual.https://www....
In the STM32L562 reference manual (RM0438), v7.0, the section 11.6.13 "GPIO register map" is missing the registers MODER and PUPDR (which are documented in the preceding sections).