STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI communication while debuging

Hi,I using STM32F407IG in IAR Embedded workbench.When I debug the program the SPI communication does not work.what could be the reason?Without debug the SPI work

Aldo1 by Associate II
  • 1556 Views
  • 15 replies
  • 1 kudos

Resolved! Target H723 with IAR EW for ARM 8.50.x

Hi, I would like to migrate a code on STM32F271 to a chip STM32H723 while using IAR EW 8.50.xMy problem is that H723 is not in the target list for  IAR EW 8.50.5I can target H723 with IAR EW 9.20 but in that way I loose compatibility with other softw...

Resolved! RTC Problem

I use the NUCLEOH563-ZI board and I want to use RTC. I configured the RTC with the LSI clock. I loaded a default date/time. On the other hand, my time does not change...My Init code :My source code to retrieve the timeThank you for your help !Ghislai...

Ghislain_Clement_0-1706261618957.png Ghislain_Clement_1-1706261681609.png

Resolved! STM32G030K6T6 fails to respond to bootloader I2C

Have STM32G030K6T6 system that in bootloader mode fails to respond to I2C.Am asserting BOOT0 pin 25, negating NRST pin 6, wait 500ms, asserting NRST pin 6, wait three seconds, then attempt to send MCU erase packet to I2C1 device address 0x57 but get ...

Remove __aeabi function

Hi guys,I'm novice in STM32, I'm working with IARIDE 850 I provided a flash memory area where I inserted two object modules which I expected should remain unchanged when I make changes to the other modules. Instead, I realized that the modules contai...

BranchCodiceMetrico.jpg
Jumper by Associate
  • 415 Views
  • 0 replies
  • 0 kudos
Labels