STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G030F6P6 TSSOP20 crystal oscillator?

As I understand, the TSSOP20 version needs an external oscillator instead of a 8MHz crystal connected directly to the MCU pins. Is that correct?I'm asking because I have seen a board on AliExpress using this same processor with a 8MHz crystal.

STM32H743VGT6 flash memory

Hi, I have bought STM32H743VGT6 and want to make bootloader and application. The issue is that its memory layout is confusing. In documentation and generated application I see/assume flash memory is:0x8000000 size 0x80000 (512kb bank1?) // bootloader...

JBond.1 by Senior
  • 73 Views
  • 4 replies
  • 0 kudos

ADC EOC wont go down after reading DR

Hi,I already tried to search for previous threads that could help me (like this one), sadly without success.I'm currently studying the ADC peripheral on STM32F3DISCOVERY from the reference manual. I started writing a simple program to measure a tensi...

Resolved! How Many G4 FDCAN Peripherals

G4 ref man says there is 1 (one) FDCAN peripheral:Yet when editing the IOC file I see 2 (two) FDCAN peripherals:I believe the ref man. What's with the IOC file editor?

mccabehm_0-1779468816269.png mccabehm_1-1779468899742.png

STM32L451 comparator settings with VREFINTx inputs

Hi All,  In my application, I am using the STM32L451RCT6 and trying to configure COMP2 with the internal Vref as a reference (specifically 3/4 Vref). For some reason, it never worked. I was only able to get it working when using DAC_CH1 or an externa...

y_liosha_0-1779367182238.png
y_liosha by Associate
  • 243 Views
  • 13 replies
  • 8 kudos

Help on STM32H753VIH6

Hello, Can someone pls help me fill this information out for STM32H753VIH6? Thank you.      Model NameCheck Group1 (注1)2 (注2)3 (注3)4 (注5)Ministerial Ordinance Article Number第6条第一号イ第6条第一号ロ第6条第一号ハCheck ItemsPresence or Absence of Radiation-Hardened Des...

Resolved! Issue with the display with ILI9341 over SPI

Hello,   ich set up my project with CubeMX for a CAN-FD (1 MBit/s / 4,8 MBit/s) and a Display for communication. Now i have the problem, that the SCK Signal for the communication looks more like a sawtooth signal than a rectangle. Also the SPI-Presca...

BNE by Associate III
  • 315 Views
  • 9 replies
  • 6 kudos