STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5 SAI in I2S mode + GPDMA

Hi,I have a board with an STM32U575 at the core.I'm attempting to set up SAI receiver in I2S mode, with 32-bit 48kHz sampling. See my configuration of SAI A below:I also want to receive the data continuously in circular mode via DMA (or GPDMA in the ...

Screenshot 2024-02-06 at 05.31.13.png Screenshot 2024-02-06 at 05.33.01.png Screenshot 2024-02-06 at 05.56.49.png
Labels