Failed to connect STM32G431C8U6 via UART (Error: GETID command not acknowledged!)
Hello,I'm trying to burn my program into the STM32G431C8U6 chip with UART on my PIN9 and PIN10.When I want to connect the chip with STMCubeProgrammer and I got the following output:08:57:10:466 : UR connection mode is defined with the HWrst reset mod...