STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Confusion with MDF and its SPI/Manchester setting

Hi all,We are trying to wire a microphone to the STM32U585. The microphone (T5838) outputs PDM and takes a clock as input.As far as I understand, the MDF peripheral supports PDM interface (as stated in RM046, Rev 4, 39.1), so it is compatible with th...

Resolved! Stoping MDF (ADF) clock output

Greetings,I'm using a low power microphone and would like to turn it off when not in use. That is done by turning off the clock to microphone, which is generated in ADF as output clock. Stopping sample acquisition (either by TRGO using window mode ac...

btd5 by Associate
  • 140 Views
  • 1 replies
  • 1 kudos
Labels