STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Milliseconds Deviations in toggling led for one second

Hi,I have been using Tim11 general purpose timer in Nucleo-f410rb micro controller board to blink an led at a delay of 1 second but there is a deviation of 18 ms in it. which have a 16 bit prescaler and 16 bit auto reload counter with it. In the .ioc...

ioc file for forum.png Screenshot from 2025-05-26 16-39-08.png

Newbie trying to Blink w/STM32H750B-DK

Hello,I acquired the STM32H750B-DK development board. Initially, when I connected it to my PC, it would power on with a display and interface. However, for the past month, it no longer turns on at all. When I connect it to my PC, a folder opens with ...

jean3 by Associate
  • 562 Views
  • 1 replies
  • 0 kudos

Resolved! usart3 on nucleo-h753 not work fine

I have been trying to transmit and receive from putty through the USB virtual com (CN1) of the core board, I tried with different baud rates and the result is always the same, garbage arrives at the putty, and I am not receiving anything either, it i...

External loader for SPI Flash for STM32WL - Fail to Init

I have a STM32WLE5 custom board with MX25L4006E SPI Flash.I created an external loader with CubeIDE based on the article - "How to add your SPI flash into the STM32CubeProgrammer’s external loader"The result stldr does not work and when I tried to de...

Egolt.1 by Associate III
  • 1838 Views
  • 2 replies
  • 1 kudos

STM32F407 I2C INA232 Problem

Hi everyone,I am using STM32F407 to read voltage and current values from INA232 and TCA9548.I have 8 INA232 so I used TCA9548 as I2C Switch.I have coded as follows:1. SET TCA9548 on Port 12. Read the voltage value on INA232 at port 1The result I get ...

Hoi_0-1700039106263.png Hoi_0-1700042387194.png Hoi_1-1700042577069.png
Hoi by Associate II
  • 1278 Views
  • 1 replies
  • 0 kudos