cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 RS485 interface with 12MBit/s

JR1
Associate II

Hello team,

is one of the STM32 MCUs suitable to run a RS485 interface with 12MBit/s? This is related to a UART interface which should be clocked by at least 192MHz.

Best regards,

Jochen Ruopp

1 ACCEPTED SOLUTION

Accepted Solutions

> For H74x/H75x, the UART speed could reach 12.5Mb/s.

IMO that's only for the synchronous mode, as that's the only mode which is then characterized in the Electrical characteristics chapter of DS (even if that chapter does not say this out aloud, that's what the diagrams and parameters are all about). And even for synchronous mode, I don't understand how would that be attained, given kernel clock -> baudrate limitation below:

The max. UART/USART kernel clock, according to Kernel clock distribution overview table in RM0433 is 125MHz and the minimum UARTx_BRR is 16, thus maximum baudrate is 7.8125MHz.

Prove me wrong.

JW

View solution in original post

2 REPLIES 2
SofLit
ST Employee

Hello,

For H74x/H75x, the UART speed could reach 12.5Mb/s. Refer to the datasheet.:SofLit_0-1726739140831.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: Be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.

> For H74x/H75x, the UART speed could reach 12.5Mb/s.

IMO that's only for the synchronous mode, as that's the only mode which is then characterized in the Electrical characteristics chapter of DS (even if that chapter does not say this out aloud, that's what the diagrams and parameters are all about). And even for synchronous mode, I don't understand how would that be attained, given kernel clock -> baudrate limitation below:

The max. UART/USART kernel clock, according to Kernel clock distribution overview table in RM0433 is 125MHz and the minimum UARTx_BRR is 16, thus maximum baudrate is 7.8125MHz.

Prove me wrong.

JW