STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Missing section IRTIM in STM32U0 RM and more.

1. According to datasheet, STM32U0 family have an IRTIM (Infrared interface). But this section is missing in RM0503. Also in SYSCFG_CFGR1 there is missing IR_MOD and IR_POL bits.2. In RTC section Figure 297 it is missing RTC_OUT2 and RTC_REFIN pins. ...

AA1 by Senior II
  • 48 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U031G8Y6TR Availability

The STM32U0 Series is very interesting, and I would like to use the small WLCSP package in a design for a new product, but the  STM32U031G8Y6 is still in evaluation. Does anyone know when the STM32U031G8Y6TR will be available for purchasing?Thank you...

vard by Associate II
  • 117 Views
  • 4 replies
  • 0 kudos

STM32l496: Clocking timer using LSCO

Hi, I wanted to clock my timer output using LSE crystal, but unfortunately only tim2 is supported with this feature. But then I saw an option of LSCO as output in cubemx, this enables the pin on MCU and according to documentation this output LSE cloc...

HZaib.1 by Associate III
  • 107 Views
  • 4 replies
  • 0 kudos

Resolved! Returning to STM32:: STM32U0 vs STM32L0

Bonjour, (in english below)J'ai travaillé sur un Nucleo-L053R8 de 2015 à 2019 (j'ai encore le Nucleo)Je reprends un travail analogue (réseau d'IoT basse énergie(LE) en milieu agricole, capteurs (certains nécessitant ADC), commandes, petits moteurs .....

Cube IDE Version: 1.15.0 failed at SystemClock_Config()

Hi :      I updated  STM32CubeIDE a few hours ago. Version: 1.15.0Build: 20695_20240315_1429 (UTC) Now it will failed at the SystemClock_Config() and missing arm_sorting.h void SystemClock_Config(void){RCC_OscInitTypeDef RCC_OscInitStruct = {0};RCC_C...

S_Ong_0-1711292059277.png
S_Ong by Associate II
  • 384 Views
  • 11 replies
  • 1 kudos

Resolved! AN6091 ('L0->'U0 migration) comments

This is not a discussion on the 'U0 as such (that'd need some time to sink in); just comment on the 'L0->'U0 migration document, AN6091. It's a very detailed and extensive document, and following items are just relatively insignificant minor issues/t...