STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401CC bootloader problem

Posted on June 28, 2017 at 14:27Hi all,i have two custom board with a microcontroller STM32F401CC in a 48pin package. One of these two micro is not working anymore due to a programmed option byte during a debug session. ST-link tell me this micro ha...

Resolved! STM32U073 flash wait states - wrong documentation

The reference manual RM0503 rev2 has inconsistent information about the flash wait states.Table 9 in §3.3.4 shows three options: 0WS, 1WS, 2WS (and, by the way, it says that all three of them correspond to "1 CPU cycle", which seems wrong).Instead, §...

SZano by Associate III
  • 1686 Views
  • 2 replies
  • 0 kudos

Unstable SPI Slave

I have a custom board with a STMWB55 (master) and a STM32F031 (slave). They communicate over SPI using DMA. Unforturenately there are communication problems.   In order to identify the problem I have simplified the setup. I have used a ST NUCLEO-F031...

Nikolaj_TL_0-1723122821437.png

Resolved! DAC output stability, performance over High temperature

I am using STM32G474VET3 controller.As i am using DAC out voltage for my application.So i want to know the  DAC output stability, performance over temperature, & the temperature drift at Maximum junction temperature 150 °C.Also any other factors affe...

sag by Associate III
  • 1419 Views
  • 1 replies
  • 0 kudos

Resolved! This question is about HAL_SPI_TransmitReceive

This question is about HAL_SPI_TransmitReceive.If a slave starts sending 8 bytes of data after the 4th byte sent by the master, is it possible to use HAL_SPI_TransmitReceive without a dummy (ignore) buffer?We will be the master side.Our assumption is...

How to determine Rx event of USB CDC ACM

Hi,I use STM32U575.The STM32U575 works as a USB CDC ACM device and I implemented it in standalone mode.OTG_FS_IRQHandler is called when data is received from the host device.Is there a way to determine that when OTG_FS_IRQHandler is called, it is due...

DK3 by Associate II
  • 1160 Views
  • 1 replies
  • 0 kudos

STM32F439 - FMC interfacing SDRAM, NVRAM and ARNIC 429

Posted on July 28, 2016 at 07:53Hi,We are developing a display using STM32F439NIH6 Microcontroller in our design.  We have the following technical queries:We have referred to your evaluation board design and we are interfacing STM32F439NIH6 with SDR...

gajraj by Associate II
  • 1602 Views
  • 1 replies
  • 0 kudos

Resolved! stm32h5 vs stm32u5 series

Hi there! I was hoping that the H5 series would be like a faster U5 series but instead they seem to be very cut down in terms of features. i.e. the H5 looks like a faster crippled U5.The U5 has graphics accelleration and HS USB but the H5 has neither...

etheory by Senior II
  • 3324 Views
  • 3 replies
  • 3 kudos

Resolved! STM32U073 - wrong documentation for clock frequency

* In the reference manual RM0503 rev2, in §5.4.4 (description of RCC_PLLCFGR), the description of PLLR[2:0] indicates:Caution: The software must set this bitfield so as not to exceed 54 MHz on this clock.* In the reference manual RM0503 rev2, in §5.2...

SZano by Associate III
  • 1368 Views
  • 2 replies
  • 0 kudos