STM32 MCUs Products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747 - DSI overflow error, no video output

Greetings!I have a board with STM32H747XI and SN65DSI84-Q1 as a converter from DSI to LVDS.The issue is that I can not get video output from MCU to 2ch LVDS panel 1920x720 with any configuration I'm trying. The main issue is that I'm getting HAL_DSI_...

VHEMaster by Associate III
  • 185 Views
  • 8 replies
  • 0 kudos

STM32U0 timer clocks x2

In contrast to the STM32L0 that I am migrating from to the newer STM32U083, the U0 clock tree (Reference manual RM0503 V2.0 figure 11) does NOT show that timer clocks are PCLK*2 when APB prescaler>1.Also, it states in 5.2.14 that timer clock TIMPCLK ...

Hans_W by Associate II
  • 83 Views
  • 2 replies
  • 0 kudos

Stm32CubeClt static Download Link

Hello,can you offer a static download link to download the CommandLineTools (Stm32CubeClt) without a Login Wall?I would like to use it to build my project in a docker container in my CI CD processGreats Peter

PPete by Associate III
  • 16 Views
  • 2 replies
  • 0 kudos

STM32H735 custom board power draw

Hi,Ive made a custom board with a STM32H735 micro on it. I have built a board with nothing but a micro and a few of its needed passive components and went to provide it power and test that its working. I supplied power from a benchtop power supply wi...

STM32N6 X-CUBE-STL

Hi,I am considering using the STM32N6 series for my next development.Are there plans to make "X-CUBE-STL" supports STM32N6 series in the near future?