STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CAN1 communication doesnt work on nucleo-l433rc-p

Hi I'm new in working with CAN-bus. My project involves two stm32 boards (both are nucleo-l433rc-p) and I want to get CAN-bus communication between them. The code is supposed to make a build in LED blink each time the blue button on the main nucleo b...

Mr4_0-1709590357897.png Mr4_1-1709590366849.png Mr4_2-1709590413932.png Mr4_3-1709590425372.png
Mr4 by Associate III
  • 3137 Views
  • 4 replies
  • 0 kudos

USB Host MTP/PTP to digital camera

Hello, I'm testing the STM3240G-eval with the USB host MTP. The goal is to retrieve the photo from a canon EOS 100.The camera uses PTP protocol.As the demonstration  code read .wav file, I wrote a wav file to the root of the SD card. The digital came...

PCu1 by Senior
  • 6442 Views
  • 7 replies
  • 0 kudos

Getting TXUNDERR while writing data to eMMC

Hello -> We are using a custom board with STM32H745 controller and 8GB eMMC communicated with sdmmc. -> getting SDMMC_FLAG_TXUNDERR bit after writing 64 bytes to eMMC. But i am giving 1k buffer array to write. -> eMMC initialization, reading logic bl...

Resolved! Nucleo-f401RE frequency measuring using timer

Hello, I am trying to create a simple frequency measuring device using 1 optical encoder and NUCLEO-F401RE board. I want to capture frequency (or period) of impulse, so I was thinking to use input capture mode and capture rising edge of impulses and ...

DSimp.1 by Associate III
  • 2828 Views
  • 2 replies
  • 0 kudos

Is there a way to do deadtime compensation

Dear all,I'm new to this forum, so apologies if I post this in the wrong category. I'm trying to find a way to implement a deadtime compensation mechanism using a STM32G4. I have a 3-level 3-phase VSI. The switching frequency is 50kHz, the deadtime i...