User Activity

Hi, I want to go to sleep/stop mode with STM32 and wake on interrupt. After last interrupt it should wait for 10sec and go back to sleep. But I see an edge case where interrupt could occur just before going to sleep/stop mode.How do I handle interrup...
Hi, I am trying to use STM32F103C8T6 standby mode and wake it up with wake up feature of RTC, but in CubeMX I don't see that this MCU would have wake up feature under RTC settings. How do I wake up this MCU from standby with RTC and wake up pin?  
Hi, I have STM32F103 and STM32F411. I have successfully made HID mouse on STM32F103, but when I try to make the same on STM32F411, the mouse does not work: "(Code 43) A request for the USB device descriptor failed".What could be the problem?The code/...
Hi, I have STM32F407 and trying to read/wirte from/to SD card and often the code get stuck in the this loop: static uint32_t SD_FindSCR(SD_HandleTypeDef *hsd, uint32_t *pSCR) { //... while(!__HAL_SD_GET_FLAG(hsd, SDIO_FLAG_RXOVERR | SDIO_FLAG_DC...
Hi I have STM32F407 and after updating STM32CubeMX 6.6.1 -> 6.9.2 I faced the same issue with SD card:https://community.st.com/t5/stm32cubemx-mcus/sdcard-does-not-work-fr-not-ready-when-migrating-from-fw-f4-v1/m-p/115499#M3876It seems that with previ...