I am starting some test with this modulehttps://it.aliexpress.com/item/1005002482177244.htmlwith 7” lcdI have found only one example that run but with TouchgfxI have got the same ioc from this example to generate a new code and insert the functions t...
Here my new code to use encoder with STM32First search on datasheet 2 pins with TIMx_CH1 and TIMx_CH2.In my case was a STM32F469 and I have used PC6 and Pc7 with TIM8_CH1 and TIM8_CH2.After search in the file stm32f4xx_hal_gpio_ex.h the relative AFx ...
A new info, starting from TouchGfx project I have made 2 simple modifications //MX_TouchGFX_Init(); <<<<<<<<<<<<<<<<<BSP_LCD_Init(); // add nowBSP_LCD_Clear(0x00FFFF00); // add now void StartDefaultTask(void const * argument){HAL_TIM_PWM_Start(&htim...