User Activity

I am using CubeIDE version 1.16.1 to program and flash a STM32F433 MCU.I am using a SEGGER J-Link flasher.When I try to run the application I get the following error:I have tried to manually set the workspace toolchain to local in the toolchain manag...
Hello,I am trying to use the DFSDM module on the Nucleo-H743ZI2 board .As a minimal example, i tried to use a sinc filter of 2. order with a FOSR of 4.Channel0 is activated in the parallel mode, standard data packing mode and the setting to take data...
I have two machines with Cube IDE installed. On one there is version 1.6.1 and the other is 1.7.0I want to update both to be able to open .ioc files from a college that has the 1.8.x The proxy settings are setup rigth because i am able to get the new...
Kudos from