STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0 FDCAN reception interrupt doesn't trigger

Hello everyone, I'm a beginner in the FDCAN field with STM32. I'm trying to establish communication between two custom boards equipped with the same CAN transceiver. The mode is normal FDCAN. Here's the configuration of the FDCAN module for completen...

seba21 by Associate II
  • 3059 Views
  • 1 replies
  • 0 kudos

Resolved! FDCAN Retransmission without blocking Bus

I have a CAN Network with several nodes. Each nodes sends only a ACK when the message was ment for it. Lets say I have nodes A, B and C.Node A wants to send the message with ID 0x5. Node B ignores this message. Node C accepts this message (sends Ack)...

MStud.4 by Associate
  • 2284 Views
  • 1 replies
  • 1 kudos

FDCAN Not working oh H755zi

Hello everyone, I'm currently facing a puzzling issue with the Flexible Data-rate Controller Area Network (FDCAN) on the STM32H755ZI board. Despite using the exact same code that works flawlessly on the STM32H753 board, I am unable to get the FDCAN t...

macsdeve by Associate
  • 1622 Views
  • 1 replies
  • 0 kudos

Resolved! FDCAN with GPDAM.

Hi, i am looking for to use FDCAN by using GPDMA . I am using STM32H5 MCU for my application. it is not clear to me how can i use GPDMA with FDCAN. please guide me__PRESENT

Resolved! CAN frame's losses

Hello all,   I am trying to receive CAN frames from a BMS, each frame is sent every 100ms and i am running the MCU's clock frequency at 180MHz (max speed) for Nucleo F446RE. Unfortunately, i am missing some frames randomly and it makes my stateflow n...

Erwan03 by Associate III
  • 2452 Views
  • 3 replies
  • 0 kudos

Ethernet uart flow problem with clock

void tcpsend (char *data) { // send the data to the connected connection netconn_write(conn, data, strlen(data), NETCONN_COPY); // relaese the semaphore sys_sem_signal(&tcpsem); } // //void HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle) ...

Kuttay by Associate III
  • 625 Views
  • 0 replies
  • 0 kudos

Resolved! ADC Linear Calibration Address

I understand that ADC Linear Calibration is performed during device production and the values stored in the System Memory.However, I have been unable to find any documentation on where the 6 values are stored.Also, are their 6 values per ADC device (...

NBrick67 by Associate II
  • 2329 Views
  • 3 replies
  • 1 kudos