User Activity

Hello,what would happen if I have a fixed 5V output L6920D boost converter and the input voltage is 5V. Will it just pass through?Thanks
Hello,I am using STM32G491 FDCAN modules 1 and 2 in bare metal. While everything works perfectly on CAN2 the interrupt on CAN1 is constantly disabled. And I do not mean the flags but the actual interrupt does not fire. Each time the interrupt for CAN...
Hello,I implemented a FDCAN in bare metal on the STM32G491 that works on FDCAN1 (with one unrelated problem). Now I need the second one too. So when I try to send over FDCAN2 only garbage comes out on the CAN bus. Yet the CRC is correct so it is actu...
Hello,I am trying to implement a USB HID keyboard on an STM32F042 without HAL or LL, just simple register defs. I took an example code generated in CubeIDE with HAL and a few other examples. I extended the example with HAL to also implement the LEDs ...
Hello,I have a strange problem that I already lost a lot of hair over. I am using cubeIDE with an stlink v2 (STM32G441 with a blank C/C++ project and CMSIS). All run very well until today. So I am sure the code itself is ok.If I compile the project b...
Kudos from