cancel
Showing results for 
Search instead for 
Did you mean: 

TCS peripheral

marekvecera
Associate

Hello,
I have custom board with STM32F301R8T6 and connected 4 channel slider sensor. I want to copy an example present in STM32CubeIde called TouchSensing_Linear. There in the configuration files such as tls_user.c, tls_user.h are includes for tls.h and tsl_acq_tsc.h, i suppose are library files for STM32_TouchSensing_Library. When i copy the code into my existing project, there is unresolved inclusion
My question is, how do i include the whole STM32_TouchSensing_Library in my project so all inclusions are resolved. Also, if I have to copy it from the example, where do I put it? In the Inc folder (which is on the same level as Src)? The library I found in the examle project has only tls.c files without the headers, or I found out so far, will it be a problem?
Thanks for answers,
Lost engineering student

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
marekvecera
Associate

solved