STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RTC freezes when STM32G030C8 is powered by VDD

I'm using the STM32G030C8 for one of my projects and i realize that in some cases the RTC stops when the power supply is up. While in VBAT supply the resonator works well and provide the correct date and time, but when i use the power supply the reso...

gtimmen by Associate II
  • 330 Views
  • 5 replies
  • 3 kudos

Resolved! VBAT & RTC Issues on Circuit - STM32H563ZIT6

I am experiencing issues with the VBAT pin on the STM32H563ZIT6 microcontroller. Specifically, the VBAT pin is not responding properly. I am using a CR2032 CMOS battery for RTC backup, but it is not maintaining the date and time as expected. When the...

VBAT_CKT.png CMOS Battery.png

Resolved! Nucleo - F207ZG RTC Time Drift

Greetings Everybody, I have Nucleo - F207ZG board. I have attached external 3.0 V coin battery to VBat and GND. I am configuring board for RTC peripheral. After configuring RTC time and again rechecking after 1 day the time starts to move ahead or ti...

Resolved! RTC Time Drifts Even Though LSCO looks good

Hi Everyone, I have a project utilizing a STM32G030F6P6 with a 32.768kHz crystal and the LSE to source the RTC clock. It is exhibiting 2% clock error (which is huge!) over a 10 minute period despite using a 20ppm crystal. I am measuring this error by...

kile by Associate II
  • 545 Views
  • 11 replies
  • 4 kudos

L4 TAMP registers resetting

   Any suggestions as to why power down, then reconnect debugger (JLINK pro) is clearing the TAMP registers to 0?Device is STM32L4P5The clock source seems to be present, it doesn't enter the if statement   if (LL_RCC_GetRTCClockSource() != LL_RCC_RTC...

_EFrie by Associate III
  • 149 Views
  • 0 replies
  • 0 kudos

Error stm32G030 not specified in the errata file.

When using RTC, the GPIO pin state of PA4 may be corrupted. RM0454, section 23.3.3 says: "In addition, it is possible to output RTC_OUT2 on PA4 pin thanks to OUT2EN bit. Thisoutput is not available in VBAT mode. The different functions are mapped on ...

PBobo.1 by Associate II
  • 678 Views
  • 5 replies
  • 1 kudos
Labels