User Activity

My main computer died and I tried to install STM32CubeIDE on a spare computer. During the installation process I received the following error message:"NSIS ErrorError launching installer"Computer: Firebat Mimi PC, Model S1, CPU Intel N100, RAM 16GB. ...
When using RTC, the GPIO pin state of PA4 may be corrupted. RM0454, section 23.3.3 says: "In addition, it is possible to output RTC_OUT2 on PA4 pin thanks to OUT2EN bit. Thisoutput is not available in VBAT mode. The different functions are mapped on ...
I recently installed the latest STM32CubeMX. Much to my great regret, I did not find the ability to generate code for the Keil / IAR IDE. Is this option really no more, or has it been hidden? If not, which of the latest STM32CubeMX versions has these...
I created a new project in STM32CubeIde (STM32F401, USB Host MSC). I haven't added a single line of my code yet. When I try to compile the project, the error appears:../Middlewares/Third_Party/FatFs/src/option/../ff.h:29:10: fatal error: ffconf.h: No...
Kudos from