STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745XIT6 MT25QL256A External Loader not working

Hi every one ..I designed custom board for stm32h745xit6 .My TouchGFX working fine with internal flash .The core board has mt25ql256a and connected as under PB2 CLKPG6 NCSPF8 D0PF9 D1PF7 D2PF6 D3I generated STLDR as explained in ST videos tutorial.my...

_legacyfs_online_stmicro_images_0693W00000dDVHjQAO.png _legacyfs_online_stmicro_images_0693W00000dDVHoQAO.png _legacyfs_online_stmicro_images_0693W00000dDaFdQAK.png
INaee.1 by Senior
  • 1552 Views
  • 5 replies
  • 1 kudos

Resolved! Do .bin files use relative or absolute addresses?

I am trying to set up a dual boot system using a bootloader in stm32F7 without using the dual bank operation. I have the bootloader, which can flash the bin files directly to the flash .My concern is whether .bin files contain any address information...

How Segger J-FLASH configures its external loaders?

A customer has a board with STM32F746 and QSPI flash.The board looks as derived from STM32746G-DISCO, though I'm not 100% sure.Their program has data in the QSPI flash, and they flash the app using J-LINK and Segger J-Flash.​Now, I cannot figure out ...

0693W00000QMxGzQAL.png
Pavel A. by Evangelist III
  • 6753 Views
  • 3 replies
  • 0 kudos

hello, I am using stm while controlling a device and after working conditions for a while, I saw that the software made itself like this. I have not encountered it on other devices. When I put the software on the processor again,it gets fixed,what reason?

That is part of broken softwareD8 0A 00 20 CD 02 00 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ...

0693W00000Lz1QVQAZ.png

External Flash Loader don't work

Hello, I am developing an external flash loader using Spi (W25Q16DV) with Stm32G070.Yes, the operation is going well without any problems.However, the peculiar thing is that it doesn't work when you write the user program in the internal flash and ru...

lhwa .1 by Associate II
  • 3646 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H750VBT6 & CubeMX & IAR

Hi everyone ;I am having a strange issue with IAR . I configured the mcu via cubemx and generated it then I build all the files but I got the errors in the attached files when I try to download the code into the MCU . But I don't get any issuse with...

BG1 by Senior
  • 1114 Views
  • 7 replies
  • 0 kudos
Labels