Hi every one ..I designed custom board for stm32h745xit6 .My TouchGFX working fine with internal flash .The core board has mt25ql256a and connected as under PB2 CLKPG6 NCSPF8 D0PF9 D1PF7 D2PF6 D3I generated STLDR as explained in ST videos tutorial.my...
Hi ..The problem was solved since I managed to develop my own ex-loaders .BTW ..Here is my custom designed board with STM32H745XIT6 & 1024X600 RGB TFT with TouchGFX.CM4 running Modbus Master RTUCM7 running TouchGFX with 256MB SDRAMHere is TouchGFX , ...
Hi ...For screen changing in sequence or jumping to any screen , Interaction feature is used.I use 2 Interactions for each screen (accept first and last screens) as NEXT_SCREEN & PREVIOUS_SCREENFor NEXT_SCREEN Interaction , below is exampleFor PREVIO...
Hi ,,You can add image in container .then you can add that container on all screens.Later , if you edit the container ,, it will automatically updated on all screens.Here is my latest TouchGFX experiment on Samsung Tab 3 10.1" 1280x800 TFT.I added 2 ...
Hi ,,,Osman recommended video tutorial is very informative.do you want to use DSI LCD which is onboard ? or you want to use generic LCD with RGB interface ?My tips ,, Divide the MX Project in 2 parts / steps .1. Configuring the TFT of your desire int...
Hi ..here is my custom designed board with STM32H745XIT6 & 1024X600 TFT with TouchGFX.CM4 running Modbus Master RTUCM7 running TouchGFX with 256MB SDRAMHere is TouchGFX , running on SAMSUNG TAB3 7.0 ,, 1024x600 , LVDS LCD & TouchGFX (STM32F429i-DISCO...