I am using the B-L475E-IOT01A kit, but I am not able to find any BLE scanning example. I want to detect beacons around me and their details as well i.e RSSI, etc.Can anyone help me regarding this?
Hi. I received a board in production state with FUS 1.1.1 BLE STAK 1.8.0 This board has a function to log data into flash peridically. Most of our board working well but this board fail to log data after few minutes from power on and BLE stack looks ...
The connection green led indicator doesn't twinkle, it is alway on and I can't see the nucleo in the ST BLE Sensor app. I suppose that the problem is with the CPU 2. I was debugging the code and it nevers reaches the function APPD_EnableCPU2( ); beca...
Android version fails to connect with "error during the connection with the node XYZ". I have tried both latest version available in Google Play Store (v4.14.7) and the other version (v4.14.4) available on ST Micro website. Does anyone have solutions...
I followed the LAB of the course on mesh networks and I am able to add the device to the mesh network. I use the ST BLE mesh App. The problem is that when I try to turn on the LED the application goes into a loop.
Hi I'm working with STM32WB5MMG-dk. The purpose is to develop BLE Gateway. The module has a custom GATT svc with 4 GATT char svc which sends and receive bytes, this data is been provided by MSP430 to STM32WB5 vice versa. So MSP430 acts as master whe...