User Activity

I Have updated the Dongle's fuses to 1.2.0 version. I did a successful test with the example of transparent mode and the monitor RF. Now I'm trying to use it as Server in a p2p example and it doesn't works. To discard, I flash it again with the examp...
I want to have 4 diveces as peripherals, each of one with a button, that they comunicate the button state to a 5th device (a Central) in a determinated period of time. The peripfherals should turn off the anttena (or save battery us much as they can)...
Im' following this tutorial of STM32WB55: https://www.youtube.com/watch?v=CKYWy7LKL68&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=19&ab_channel=STMicroelectronicsAll is fine until I try to generate code. It gets stuck at the moment of "Copying libr...
The connection green led indicator doesn't twinkle, it is alway on and I can't see the nucleo in the ST BLE Sensor app. I suppose that the problem is with the CPU 2. I was debugging the code and it nevers reaches the function APPD_EnableCPU2( ); beca...