STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UCPD SINK Application NUCLEO-u575ZI-Q

I'm trying to run a simple UCPD SINK application on the NUCLEO-U575ZI-Q.I attempted to follow the example provided here: https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink#-5BOPTIONAL-5D_Conf...

acipriano_1-1713372587747.png acipriano_2-1713372661433.png

STM32F103CBT6 not recognized USB device

It is not recognized as a USB device. What did I do wrong or miss?IC: STM32F103CBT6 1. Is the distance between USB D+ and PA12 (Pin 33) and USB D- and PA11 (Pin 32) long?The distance from USB D+ to PA12 and USB D- to PA11 is approximately 35 mm (1,38...

CXR_0-1713470218159.png CXR_1-1713470237176.png CXR_2-1713470250179.png CXR_3-1713470264226.png
CXR by Associate II
  • 80 Views
  • 3 replies
  • 0 kudos

CAN Bus doesn't work in normal mode between two MCUs

Hello,Hope you all doing well..!! I am using two microcontrollers i.e., for transmitting data I have to use STM32F407VET6 and for receiving I have to use STM32F407VGT6 also I have to connect MCP2551 CAN Transceiver. I am transmitting data from one bo...

mr_vineet by Associate II
  • 574 Views
  • 22 replies
  • 9 kudos

Error Target MCU stm32f401cd

Salut la communauté, J'ai créé une carte électronique permettant de visualiser l'état de la batterie d'un ULM. J'ai utilisé le microcontrôleur STM32F401CD, et j'avais initialement prévu d'utiliser uniquement l'horloge interne HSI du MCU, donc je n'ai...

yassir by Associate
  • 74 Views
  • 4 replies
  • 1 kudos

SD card doesn't work with stm32L552ZET6

Hello everyone,I have been using for a long time the stm32L496ZGT6 in a customized PCB with an uSD card module. Never had any problem interfacing the card. Due to the shortage of supply during the pandemic situation I bought a couple of stm32L552ZET6...

tarm123_2-1700225538973.png tarm123_3-1700225605219.png tarm123_4-1700225637176.png tarm123_0-1700225232010.png
tarm123 by Associate
  • 325 Views
  • 2 replies
  • 0 kudos

STM32f071RB PA1 Comparator

Hello!I'm using Comparator 1 in the STM32f071rbt6 uC. The Comp  is properly configured, and sends an interrupt once triggered on PA1 referenced to PA4(DAC_OUT_1).it happened that the PA1 GPIO accidentally was not configured. Yet the comparator functi...

tage by Associate
  • 48 Views
  • 1 replies
  • 0 kudos