STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

help:confused between cortex m4 platform

Posted on March 03, 2013 at 11:52hi everyone i am looking forward to purchase evaluation board for learning cortex m4. i would be requiring GLCD/TFT and camera in future for some image processing applications where i might be using DSP capability of...

LD 7 remains switched on

Posted on March 04, 2013 at 07:45HiRecently I was using my STM32F4 discovery board in my variable speed drive project and got an over-current detection message in the IAR, and LD 7 (Green LED at the bottom of the board) lit up.Now, I think I did not...

STM32F4DISCOVERY, USB USE_ACCURATE_TIME

Posted on February 25, 2013 at 21:49 Hi, I use a STM32F4DISCOVERY, and I would like to begin to understant how the USB HOST/OTG works... ands it's not easy, there is a lot of files and lines of code. I saw in ST examples, that in s...

keypad 3x4 rs 130404

Posted on March 02, 2013 at 23:19 Hi, i try to use a keypad with my stm32vldiscovery but it doesn't work can u help me? i connect first 4 pin to stm32vldiscovery in PA0-PA1-PA2-PA3 in output open drain, and last 3 pin to PA4-PA5-PA6 as analo...

Minor error in stm32f4x7_eth.h (ethernet)

Posted on March 03, 2013 at 10:14In the header file ''stm32f4x7_eth.h'' bit 0 of RDES0 is defined thus:/*!< Rx MAC Address/Payload Checksum Error: Rx MAC address matched/ Rx Payload Checksum Error */#define ETH_DMARxDesc_MAMPCE      ((uint32_t)0x000...

UART4 on STM32F417

Posted on March 01, 2013 at 16:25Hi Guys, After reading the whole of Google and finding this thread (https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%...

Delay function with timer

Posted on February 22, 2013 at 09:12Hi, I am trying to make a simple delay function using a timer but i get weird results .Here is some of the code void TIMERS_init(){   TIM3->PSC = 23999; // f timer = fclk / 24000 => 1kHz TIM3->ARR = 0xFFFF; TIM3->...

raducara by Associate II
  • 2999 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.