STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Facing unknown runtime error

Getting this error "assertion "Balloc succeeded" failed: file "/build/gnu-tools-for-stm32_10.3-2021.10.20211105-1100/src/newlib/newlib/libc/stdlib/mprec.c", line 778" in runtime for stm32l452ret6p microcontroller. I am doing baremetal programming and...

SSaiy.1 by Associate III
  • 2676 Views
  • 3 replies
  • 2 kudos

Resolved! STM32L496QGI3 Vbat pin connection

Hi, Can the VBAT pin on this part be left floating? I currently have the pin disconnected. Or should it be tied to VDD or GND in order for the part to function properly?  Thanks,   

VBAT.PNG
WAkba.1 by Associate
  • 1470 Views
  • 1 replies
  • 0 kudos

Terminal flickering when sending characters through UART

Hello,I am attempting to create a guitar hero-style game using the B-L4S5I-IOT1A board. I have an array representing the notes to play and wish to update the display every 125ms with a new gameplay frame (a given frame has the next 10 notes the user ...

Marxellus_0-1712590661426.png Marxellus_1-1712590834235.png Marxellus_2-1712590856688.png Marxellus_3-1712590893131.png
Marxellus by Associate II
  • 3511 Views
  • 6 replies
  • 1 kudos

STM32 software library for implementing a sensor hub

Hi, I want to implement a sensor hub that can connect to multiple (e.g. 8 ) sensors (from the same type), collect data from them, aggregates the data into a single message and sends it out. The board will be custom, if necessary, and based on e.g...

kreceon by Associate
  • 1466 Views
  • 0 replies
  • 0 kudos

STM32H563 LSE does not always start

I am using an stm32h563 nucleo 144 board, and I am frequently running into the issue that after a power cycle the LSE does not start.This is the relevant part of my SystemClock_Config: LL_PWR_EnableBkUpAccess();while (LL_PWR_IsEnabledBkUpAccess () ==...

PieterG by Associate III
  • 3337 Views
  • 5 replies
  • 4 kudos

Resolved! Debugging STM32H573I-DK_aws_ri_tz example

Hello everyone, I hope you are well.I'm starting a new project using the STM32H573I-DK kit, where I would have to connect to AWS and publish the value of some sensors. The first step was following the webinar https://content.st.com/stm32h5-connects-s...

ffjunq_0-1712674300595.png ffjunq_1-1712674359741.png ffjunq_2-1712674375086.png
ffjunq by Associate III
  • 1271 Views
  • 1 replies
  • 0 kudos

STML496RGT from SPI to QSPI

Hi all!I'm currently programming a pulser and have to write a list of registers. I prepared the communication on SPI (which works), only to realise the pulser can only be programmed over QSPI.Now I'm having some issues switching my code from SPI to Q...

Untitled (21).png Untitled (19).png Untitled (20).png Untitled (22).png

Resolved! SPI by hand/prerequisites for SPI

Hi,I've been trying to adapt the current SPI driver in RIOT OS to support the U5 series(STM32U585AI), due to my lack of success I've been trying to sidestep RIOT for a moment and try to do must of the setup manually. But so far I have not been able t...

mdr by Associate
  • 2197 Views
  • 3 replies
  • 0 kudos

Resolved! STM32G031C6 problems during production programming

Dear all,In the last weeks we have started the production process of a specific equipment, using the new microcontroller STM32G031C6 and unfortunettly we have faced some problems after the programming process.The problem is that some devices were app...

TFBorth by Associate II
  • 4133 Views
  • 6 replies
  • 1 kudos

ERR when external SDRAM & NandFlash with FMC

Hi there,I have a touchGFX project with STM32F429BI, which uses the external SDRAM for the buffer, and the Nand Flash for the image.Both SDRAM and Nand Flash work well when turning off the other.But when I enable LTDC, the Nand Flash always gives an ...

Junde by Senior III
  • 969 Views
  • 0 replies
  • 0 kudos