STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to wake-up on time in time with RTC ?

Hi eveyone,I have a problem with RTC wake up. I use LSE 32.768kHz.I run example from manufacturer to wake up MCU from Stand by mode very 1min, 2mins. Everything work okay.But, When I put delay 10s and HAL_PWR_EnterSTANDBYMode(); into while(1). Everyt...

Resolved! STM32F746-Disco, how do I enable ethernet and ping the kit?

HiWe are trying to use the f746 disco kit as a udp server that writes what it receives to an SD card. The kit is currently connected directly to a PC with ethernet and usb. As this is our first stm project, we tried following several tutorials that a...

moaNTNU by Associate
  • 2082 Views
  • 3 replies
  • 1 kudos

Resolved! stm32l431rct6: SD detect pin question

Sorry, are there has a pin call or used for SD_detect in Stm32l431rct6? I can not find in STM32L431xx Datasheet - production data. These has no mention.I do not know which pin(SD-Detect)should i choose for GPIO_Input of the FATS.

Jacob3104 by Associate II
  • 1308 Views
  • 1 replies
  • 1 kudos

Mems microphone and stm32 f4 boards

Hi  techteam,Please provide and reference code example or community project which contains how to interfaces st pdm microphones with pdm /i2s/Sai peripheral of nucleo f446re board.Please note I have already went throught the appnote an5027.Waiting fo...