User Activity

Hello, this is LewisI have a question about "STUSB4500 NVM Customer Sector0-4 Write".I would like to know the message below from the technical note "STUSB4500 NVM Register Description and General Access".(attach file)"Load NVM data sector 0 (8 bytes)...
Hi I am luis.I'm testing TouchGFX and have a question.1. Create a custom board project with TouchGFX V4.22.1 Designer2. Move the STM32F769I_DISCO.ioc file in the project created above to the STM32CubeIDE folder in the project, then run STM32F769I_DIS...
Hi I am luis.I'm testing TouchGFX, and I have a question.After creating an example board project with TouchGFX V4.22.1 Designer and then moving the STM32F769I_DISCO.ioc file into the STM32CubeIDE folder to set the IO, an error occurs when compiling a...
Hello I'm luis.I wanna to control new LCD(partname WF50DTYA3MNN0, MIPI-interface). show attached file.But I have problems how to setting TouchGFX many parameters about WF50DTYA3MNN0. please help me. Even if it takes some time, please let me know step...
Hi. I am luisI have question about STM32F413CGU6 FW upgrade using USBQ1. how can I setting Stm32CubeIDE usb parameters?? FW upgrade is only use "OTG"??I can use USB mode only "host" or "device".Q2. Is there another setting for standalone USB setting?...