Skip to main content
Associate II
August 18, 2023
Solved

STM32H735 ADC3_INP16 Issue

  • August 18, 2023
  • 8 replies
  • 3360 views

The data sheet for the STM32H735 (DS13312) lists "ADC3_INP16" as an additional function for PH5, and this function is also available for selection in both STM32Cube IDE and STM32CubeMX.

However, in looking at the STM32H735 reference manual (RM0468) , the ADC3 connectivity figure (29.4.4 Figure 231) does not list ADC3_INP16.

ADC3 has 19 total inputs (external inputs 0..15 and 3 internal inputs for vbat, vsense, and vrefinit),

What is the purpose of ADC3_INP16 as an additional function on this pin?  It seems unlikely that the IDE and data sheet both contain this same error, but in reading the documentation I cannot understand what the purpose of using the pin for this function would be.

Thank you.

This topic has been closed for replies.
Best answer by KDJEM.1

Hello @dsurrett ,

The documentation issue is fixed in DS13312 Rev 4.

Edit: The STM32CubeMx is solved in STM32CubeMX 6.11.0.

Thank you for your contribution in STCommunity.

Kaouthar

8 replies

TDK
August 18, 2023

I would bet it's a typo in the datasheet that the CubeMX programmers just followed.

It's also in the STM32H743 datasheet, but isn't selectable in CubeMX for that chip.

"If you feel a post has answered your question, please click ""Accept as Solution""."
KDJEM.1
ST Technical Moderator
August 21, 2023

Hello @dsurrett and welcome to the community :),

Thank you for bringing these issue to our attention.

I confirm this confusion  and I will check internally.

@TDK Could you please precise which STM32h743 package that had a contradiction between the STM32CubeMX tools and the datasheet? Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
TDK
August 21, 2023

I just googled "stm32h743 datasheet" and clicked the first link. Not sure which package, probably all of them that PH5 is present on.

TDK_0-1692624344601.png

https://www.st.com/resource/en/datasheet/stm32h743vi.pdf

"If you feel a post has answered your question, please click ""Accept as Solution""."
KDJEM.1
ST Technical Moderator
August 21, 2023

Hi @TDK ,

Thank you for this detail.

I checked TFBGA240 +25, LQFP208, LQFP176, UFBGA176+25 and UFBGA169 packages for STM32H743 and I don't found any contradiction between RM0433, datasheet and STM32CubeMX for ADC3_INP16.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
ST Technical Moderator
August 21, 2023

Hello @dsurrett ,

The ADC3_INP16 not connected to PH5. 

The datasheet and the STM32CubeMX are wrong.

I reported this issue internally.

Internal ticket number for documentation update: 159618(This is an internal tracking number and is not accessible or usable by customers).

Internal ticket number for STM32CubeMX update: 159625(This is an internal tracking number and is not accessible or usable by customers).

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
dsurrettAuthor
Associate II
August 22, 2023

@KDJEM.1 thank you for confirming!

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
January 4, 2024

Hello @dsurrett ,

The documentation issue is fixed in DS13312 Rev 4.

Edit: The STM32CubeMx is solved in STM32CubeMX 6.11.0.

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.