STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EMW3080 not working properly

Hi,I flashed an EMW3080B module with this firmware ST-EMW3080B_V2.1.11_SPI.ALL from this location on another board not B-U585I-IOT02A. It is connectet to SPI from STM32. Problem is next: when MCU set pin 11(CHIP_EN) from EMW3080B to HIGH to enable mo...

MZamu.1 by Associate
  • 157 Views
  • 0 replies
  • 0 kudos

Debugging STM32H7B3I-EVAL with ETM

Hi,I wanted to debug my STM32H7B3I-EVAL board with J-Trace Pro through ETM interface. According to the manual of STM32H7B3I-EVAL, to enable ETM, R69 must be removed to avoid conflict with the WIFI_SPI4_MISO output, and it's also recommended to remove...

JSHI.1 by Associate
  • 83 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H7BI3-DK WiFi Not Working

Hi,I have been writing drivers for the ISM43341-M4G-L44-SPI WiFi module mounted on the STM32H7BI3-DK.I can send the device AT commands and get back the OK response, but after setting the network parameters SSID, password, security mode, DHCP after is...

B-U585: Qualify SSID with space: Not good!

Hello,the B-U585 Demo when asking for the SSID qualifies a name with a spacebar. Problem is, that many SSIDs contain a space by itself, like "FRITZ!Box 7530 ..." or "Galaxy ...". As the application does not echo what is sees, useres are left in the d...

set up wifi with sdio

Hello Every BodyDoes any one have any code for setting up Wifi with sdio?My micro is STMF412 and My wifi module is JC-TSM89ES (Realtek RTL8189ES) Single Module.

Ybaya.1 by Associate
  • 94 Views
  • 0 replies
  • 0 kudos

How to send data via WiFi through a softAP?

Hello,I am struggling to send data via a softAP over WiFi. Setting up the softAP and connecting to it from another device works well. Now, I would need to bind the newly created socket to the desired port and that's where it fails for me. I don't kno...

BBecs.1 by Associate II
  • 205 Views
  • 5 replies
  • 0 kudos