STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-H503RB Problem of DAC

Hi, ST community.I'm trying to drive a motor using Nucleo-H503RB.At that time, I want to use DAC pin to watch variables, but I have problem of DAC.<Detail>To use the DAC, I set the PA5 to the DAC in Motor Workbench.I confirmed that when the DAC is se...

Kota by Associate
  • 1197 Views
  • 1 replies
  • 0 kudos

STM32F407G Disc: TIM input encoder mode

Good afternoon community,I am trying to implement the Input Encoder in STM32F407G Discovery board.I implement all things, but I am not able to generate desired the output from the board.I get counter/count/position value as zero.   Can you please he...

MG1_0-1710159725167.png
MG1 by Associate II
  • 2547 Views
  • 4 replies
  • 0 kudos

NUCLEO-L476RG SDMMC FATFS DMA 4-bit wide mode issue.

Hi,I have configured the Nucleo-L476RG to write to a 64GB exFat Micro SD Card in 4-bit mode using DMA.This appears to work correctly once I navigate around the still present library errors which prevent you from initialising in SDMMC 4-bit mode. You ...

Gavin_2024_0-1710250915486.png

Falling of digital signal after some delay

Please find the image for the reference.Falling time of digital signals should in nano second, but here its almost taking 42usec. I have configured GPIO mode as Alternating Push and Pull, Pull down.let me know how to reduce the falling time.

IMG_20240306_155433575.jpg
Sushmita by Associate II
  • 1326 Views
  • 2 replies
  • 0 kudos

Resolved! F446RE and CAN2 in loopback mode

I'm working on a custom board with a F446RET6 and testing through some code bits. I've been able to successfully test that the board programs and functions with a led-blink style program. My problem is that I'm attempting to use CAN2; I'm trying to t...

Resolved! RXNEIE needed for dma request?

Hello, i am trying to interface TI's ADS8910 (18bit SAR ADC) to an STM32F730 via normal SPI, since i am unsure whether QSPI will work.I want to achieve the full 18 bit @1MSa, which is possible when working with 54MHz (/2 APB2 prescaler on the F730 wh...

Resolved! STM32F303 USB

Hello,I'm working on a cutom made board controlled by an STM32F303ZET, I figured out that I forgot to pull up D+ for USB communication, even doing it externally keep showing me this error. I tried to pull up the D+ using 3.3V directly and also by pul...

EL_HACHIMI_0-1708698094232.png