User Activity

We are trying to use software "STM32 st-link utility" to program stm32h563 series MCU.However, it could not recognize our target MCU and shows "no target connected".Stm32h563 Target not connectedThe SWD pin connections are correct, we are able to do ...
I am using NUCLEO-H503RB as I3C Target with LL library.What's the minimum size of TX-FIFO available when I3C Target is reading by Controller?I setup I3C Target TX-FIFO using function "LL_I3C_ConfigTxPreload" with 1 byte, but it always runs 8 bytes pe...
I am using EVB NUCLEO-H503RB with I3C Target feature. I have successfully assign a dynamic address (0x50) to this I3C Target: However, I could not get ACK from this Target with Address 0x50:   Below are my configure, is there anything missing for res...
I have a EVB NUCLEO-H503RB and tried to implement I3C Target feature. Before testing on I3C system, I would like to test some basic read write with legacy I2C Controller. However, I just found that it seems to be not support with static address on I3...
Kudos given to