STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

equivalent application note

HI, Is there an equivalent application note or similar information about sleep modes for the F0 series?https://www.st.com/resource/en/application_note/an4365-using-stm32f4-mcu-power-modes-with-best-dynamic-efficiency-stmicroelectronics.pdfCheers, Cla...

Resolved! Stm32 azure rtos

Hi, I am new to stm32 microcontroller. I am finding difficulty to render my html page using azure rtos. As I have seen the example of stm32f429zi nx_Webserver. First of all  I could not find html files in the example folder.However with other GitHub ...

STM32H5 I3C Target don't send ACK when receive header

My I3C target don't send ACK after controller send an arbitration header ,and it will generate a DOVER flag and ERRF flag. ex.Send HAL_I3C_Ctrl_IsDeviceI3C_Ready before controller transmit data.Send HAL_I3C_DIRECTION_READ and so on

Sunwaz by Associate III
  • 2305 Views
  • 4 replies
  • 0 kudos

3-wire SPI Configuration

Hello,Currently i'm working on STM30F030 controller.I want to connect TFT display with this controller, display has three pin for SPI (SDA,SCL & CS) and used only for write operation.so how to configure controller for 3-wire SPIIf i have to connect...

SPraj.15 by Associate II
  • 2119 Views
  • 2 replies
  • 0 kudos

Rare UNALIGNED hard faults on STM32H753ZI

I have project on STM32H753ZI and I am using ADC in DMA mode. Every few hours I get Usage Fault Unaligned access hard fault. Fault is invoked in my ADC_ConvCptlCallback in which depending on ADC value I decide about GPO stateStack during HardFault:Ha...

kicur by Associate II
  • 2856 Views
  • 3 replies
  • 0 kudos

STM32F446 USB

Hi,Just started working on a project based on the STM32F446RET MCU. Using the CubeIDE framework (code generated from .ioc file) and having some trouble with USB OTG FS Device mode. If I enable VBUS sensing, then the  USB doesn't enumerate. What's not...

alexxs by Associate II
  • 1571 Views
  • 1 replies
  • 0 kudos

F4 HAL CRC utility

Hi , have somebody link to exe or online or linux utility with same result as HAL CRC calculate? 

MM..1 by Chief III
  • 2763 Views
  • 6 replies
  • 0 kudos