cancel
Showing results for 
Search instead for 
Did you mean: 

VREFBUF not working on STM32WLE5JC

grf14
Associate

Hello everyone,

I'm trying to set up VREFBUF as an internal reference at 2.5V, but the configuration isn't working. I've seen there were issues with this (VREFBUF Enable Problem - STMicroelectronics Community), but even after rearranging the function 'HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);', it doesn't work properly. I'm using the STM32WLE5JC on the 'Lora E5 mini' development board. Here is my code:

void HAL_MspInit(void)

{

/* USER CODE BEGIN MspInit 0 */

HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);

/* USER CODE END MspInit 0 */

 

/* System interrupt init*/

 

/** Configure the internal voltage reference buffer voltage scale

*/

HAL_SYSCFG_VREFBUF_VoltageScalingConfig(SYSCFG_VREFBUF_VOLTAGE_SCALE1);

 

/** Enable the Internal Voltage Reference buffer

*/

HAL_SYSCFG_EnableVREFBUF();

 

/** Configure the internal voltage reference buffer high impedance mode

*/

HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);

 

/* USER CODE BEGIN MspInit 1 */

 

/* USER CODE END MspInit 1 */

}

 

Any idea what I can do?"

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
grf14
Associate

I just realized that in the Lora E5 chip the Vref+ pin is connected to Vadd pin, so that's the problem, it's not possible to use VREFBUF in this chip. In case anyone face the same problem I left here the internal connections of the STM32WLE5JC.

ff8547d1c55cf7d70a3e7437f21c11a99807278c_2_666x500.jpeg

View solution in original post

1 REPLY 1
grf14
Associate

I just realized that in the Lora E5 chip the Vref+ pin is connected to Vadd pin, so that's the problem, it's not possible to use VREFBUF in this chip. In case anyone face the same problem I left here the internal connections of the STM32WLE5JC.

ff8547d1c55cf7d70a3e7437f21c11a99807278c_2_666x500.jpeg