ADC signal noise
Hi, I'm using stm32f429 disc1 adc1 PA4 and GND to get the ADC signal, the voltage of the signal is 300 mV. The signal that I'm getting after conversion has some noise, But the same signal when seen through an oscilloscope has no noise. The noise or distortions are getting generated once I connect to the pins of the powered-on board.