STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NUCLEO-L011K4 Low Level Blinky not working

I'm starting to learn about low-level embedded development. My goal is to learn how I can write my own linker scripts and startup code. I also want to learn how to use raw register calls to do something useful. I want to use the NUCLEO-L011K4 board a...

tim-hilt by Associate II
  • 6306 Views
  • 15 replies
  • 9 kudos

STM32G4 HRTIM operations of push-pull mode

I have two questions regarding RM0440 Rev.8, Figure 195:In Figure 195, it shows that the roll-over events invert the push-pull logic. A roll-over event is defined as "a counter roll-over event is generated when the counter goes back to 0 after reachi...

iy by Associate
  • 1788 Views
  • 2 replies
  • 0 kudos

Resolved! scanf over VCP on nucleo-C071RB

I am able to use the demo code as is to send characters to TeraTerm but when I try to use scanf to get inputs from TeraTerm, i get nothing. when i debug the code, i see that the function doesn't for user entries and just go to next line in the code. ...

Ali_C by Associate
  • 1658 Views
  • 2 replies
  • 2 kudos

Resolved! Problem with Pin A11 on STM32U595VJ

Hello,I've migrated an application from STM32L496VG to STM32U595VJ.Pin A11 is used as capture input TIM1_CH4.With U5 device the input on PA11 couldn't reach full level at 3.3V. I have the same behavior with 5 MCUs STM32U595VJT6 and PA11 is connected ...

STM32U595VJT6_PA11_NIO.png STM32U595VJT6_PA10_IO.png
SStor by Senior
  • 6816 Views
  • 7 replies
  • 2 kudos

Resolved! SRAM internal frame Buffer - LTDC - Strange Issue

hi,I have successfully connected LTDC display(480x272) with STM32H723ZGT6 - RGB565 mode .I could able to image file from internal Flash Memory .I could able to Load Perfect colour from DMA2D by using. framebuffer in global level .uint16_t framebuffer...

MMARI1_0-1731035396898.jpeg MMARI1_2-1731035769630.jpeg
MMARI.1 by Senior II
  • 2350 Views
  • 3 replies
  • 0 kudos

Multilevel Inverter

How generate multicarrier PWM on stm32? Currently my project is making Modified seven level packed u cell inverter.  

1000147156.jpg
Tren by Associate
  • 1045 Views
  • 1 replies
  • 0 kudos

Send data over SPI instead of serial wire debug

I am developing some trackers for personal use in VR and have found an excellent solution that meets my needs using the STM32CubeIDE environment and some boards. I create and test the files, but I realize that debugging over serial communication is n...

Syntech by Associate II
  • 4154 Views
  • 7 replies
  • 3 kudos

Resolved! STM32L496 Resetting CAN TEC/REC Counters

I have a system in which the power source to the CAN transceiver interfaced to the on-chip CAN peripheral is common between multiple MCU's vis-a-vis a connector. I have experienced issues wherein if the connection is broken and then re-connected betw...

Elliott99 by Associate II
  • 1738 Views
  • 1 replies
  • 0 kudos