Hi We are working on STM32H503 MCU which has ARM Cortex 33. In datasheet it is provided that 12 cycles or instruction to enter into an interrupt function. Configured system clock as 250MHz, with that we could reach an interrupt function within...
Hi, We are currently using NUCLEO-H503RB (NUH503RB$MR1) Eval board. We are using STM32 Cube IDE for flashing the board. Upon connecting the Eval board with USB-C cable it get detected by the IDE. But during flashing we are getting the following ...
Hi, I am currently using STM32H503KBU6 MCU (32 pins). For my project the space in PCB board is critical. I have placed a LDO, Level translator, voltage supervisor and along with their associated passives in a 10mmx16mm PCB board. Now I still nee...
Hi, I am currently using STM32H5 series, to transmit the RTC register content to an escalator base board. I need to transmit these data in a parallel manner (i.e. MCU act as a slave and the base board act as a master). I studied that STM32H5 seri...
Our MCU has been soldered on the PCB. So, we can't able to directly connect the debugger pin to the MCU. In order to connect the debugger pins we need to fan out the respective MCU pins using a 0 ohms resistors.