STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL DMA USART RX Character > Buffer Size Problem

Sure it's a small thing but I just can't get on with the UART RX via DMA. I want to use the HAL in my project and execute the following.Precondition:- UART2 initialized- DMA GPDMA1 Channel 3 Mode: normal- RX Buffer 5Bytes- character match Interrupt i...

MStei.4 by Associate III
  • 2009 Views
  • 2 replies
  • 0 kudos

how to pull down ADC pin?

hi,i am facing problem with ADC, when nothing is connected on ADC pin it still shows count. i thought may be the pin is in float condition. i pulled it down but still its showing counts. cant find the problem. 

CJami by Associate III
  • 5149 Views
  • 6 replies
  • 0 kudos
MYOKO.1 by Associate
  • 1362 Views
  • 1 replies
  • 0 kudos

Flash that goes into "Inconsistency error" during second word write in debug mode, and first write is 0 in normal run.

HelloI'm working on the implementation of a UF2 bootloader for the STM32H743ZI, and I get an issue with the flash that goes into "Inconsistency error" during second word write.I have properly erased the flash sector before the write.Here is the funct...

Switching relay causes hardFault on MCU

I am switching 5V relay with BJT using MCU(STM32G030) pin. When clock speed is 64MHz(max speed) and 1ms timer update interrupt is enabled, not every time I switched relay but sometimes MCU goes into hardFault handler. But if I disable timer update in...

SSone.1 by Associate III
  • 4317 Views
  • 6 replies
  • 0 kudos

STSW-STM32102 driver is no more adequate from Windows® 10

STM32F078 USB connection to Windows 10 reports there are no compatible drivers. The STM website says " Starting from Windows® 10, the STSW-STM32102 driver is no more adequate and the usage of the native inbox driver is recommended.How can I resolve t...

rfdmod by Associate
  • 17818 Views
  • 9 replies
  • 0 kudos

STM32H745I-DISCO STLink UART Virtual Com Port not outputting

Hello, I have a STM32H745I-DISCO board that I would like to debug using UART Serial over the STLINK virtual com port. UM2488 Section 6.14 shows this should be connected to USART3. I have the USART3 peripheral enabled with the following configuration:...

0693W00000JORC3QAP.png 0693W00000JOR6pQAH.png
woozl by Associate II
  • 3410 Views
  • 4 replies
  • 0 kudos