User Activity

Hello,I have a problem with the bootloader on a Nucleo G071RB. I have no problem reaching the bootloader to download some new firmware in UART, after a reset and Boot0 pin set as it should, the bootloader responds to messages send through UART : when...
Hello,Looking at the datasheet and the reference manual, I can't find the values of the hysteresis that can be used for the comparators, the datasheet simply states Low, Medium and High values, which is not very precise. Anyone knows the exact values...
Hello,I have a small question about the bootloader, I guess this is common to all protocols but I have only tested with USART protocol. After sending the command readout unprotect, the application note states that :"After the transmission of the [fir...
Hello,I'm testing to flash a new firmware using an ESP32 on an STM32F103xC, using the application note AN3155. There seems to be an error in the computation of the checksum that must be included in all messages. The documentation states that : 1. ...
In my design, I have two MCUs, the STM32F103RCT6 and an ESP32. At some point, the ESP32 will perform a firmware update of the STM32. So it will need to reset it through the NRST pin, controlled through a GPIO. I have checked rapidly the datasheet, th...