STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32C0 Boot Programming

Hi, I am planning to use STM32C011F6 for a simple application and want to download application through UART1. How to use BOOT0 pin to program MCU for the first time. According to data sheet, UART1 pins PA9/PA10 needs remapping to function as UART. Al...

KGane.1 by Associate III
  • 1966 Views
  • 1 replies
  • 0 kudos

Resolved! [ STM32G070 ] STM32G070 input mode pin speed setting?

Dear Sir,​In STM32G070 series, the code shows the speed setting for GPIO output,If my GPIO is setting for input to receive external interrupt, does the speed setting also apply for GPIO input mode?Thanks/** @defgroup GPIO_speed GPIO speed * @brief ...

E-John by Associate III
  • 2518 Views
  • 2 replies
  • 1 kudos

SDIO API for H7

Sorry, I am new STM32 MCU :grinning_face_with_sweat: ​I want to bring up WIFI function with SDIO to connect Internet, but I cannot find any SDIO API in H7 like stm32f4xx_sdio.c.The link is where I can find the answer I want, but it only supports H747...

wG.1 by Associate II
  • 1978 Views
  • 1 replies
  • 0 kudos

STM32F407VGTX_FLASH.ld: No such file or directory error

Hi i wanted to try new extension but i get this error. The code is a basic blink its working on cubeide but when i try on vscode this happens.Thank you already[build] c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltoo...

HSarı.1 by Associate
  • 4312 Views
  • 4 replies
  • 0 kudos

Resolved! GPIO rise/fall time on Nucleo H7

I am prototyping an application on a Nucleo H7 board and I would like to use 50 MHz SPI master for performance reasons.At lower speeds (25 MHz, for example) I am able to generate a fairly clean SPI Mclk that passes requirements, however at 50 MHz I e...

Resolved! Change ADC clock in STM32H7

Hello, i'm using an STM32H7 but unfortunately for a known bug of the firmware package i'm not able to select the ADC prescaler. Uprading to a newer firmware package is not considered.At the moment i resolved applying a prescaler with the linehadc1.In...

0693W00000aJYovQAG.png
halbeeee by Associate II
  • 4965 Views
  • 4 replies
  • 0 kudos

Counting 10000000 with 16 bit TIMER

Hello,I'm counting a 10MHz oscillator(with external clock mode 1) for 1 second using the stm32f0 processor's TIM1. I get about 10 000 000 pulses.Then the system has a starting point and I start the 1s counting process here. The timer counts a maximum...

hazall by Associate III
  • 7918 Views
  • 12 replies
  • 0 kudos

How to use oscillator as a TIMER clock source ?

#define ExternalOSCport GPIOA #define ExternalOSCTimer TIM1 #define ExternalOSCpin GPIO_Pin_8   voidClock_Config(){   TIM_ICInitTypeDef TIM_ICInitStructure; TIM_OCInitTypeDef TIM_OCInitStructure;   NVIC_InitTypeDef NVIC_InitStructure; GPIO_InitType...

hazall by Associate III
  • 697 Views
  • 0 replies
  • 0 kudos