2022-10-27 3:48 AM
Hi,
I use SAI interface for reading data: 8 of 32bit slots -> 256 Bytes
This work fine:
uint32_t GlSAI_DMA_Buff[8];
....
HAL_SAI_Receive(&hsai_BlockB3,(uint8_t *) GlSAI_DMA_Buff, 8, 0xffffff);When I use DMA like this:
HAL_SAI_Receive_DMA(&hsai_BlockB3,(uint8_t *) GlSAI_DMA_Buff, 8);It only recieve 1 Byte:
Then only GlSAI_DMA_Buff[0] is equal to 0x52 - but there should be something like 0x5260A246 , in other places are also zeros...
When I try another DMA for mem to mem (on GlSAI_DMA_Buff ) it works fine - so probably my MPU for disabling Cache is set correctly.
Any advice please?
Solved! Go to Solution.
2022-10-27 4:57 AM
OK, the Cube did not enable clock for DMA - so no DMA setting was transfered to DMA registers...
2022-10-27 4:57 AM
OK, the Cube did not enable clock for DMA - so no DMA setting was transfered to DMA registers...