Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
STM32 MCUs Boards and hardware tools
STM32 MCUs Software development tools
STM32 MCUs Embedded software
STM32 MCUs TouchGFX and GUI
STM32 MCUs Motor control
STM32 MCUs Security
STM32 MCUs Wireless
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
GNSS positioning
AutoDevKit Ecosystem
Edge AI
Analog and audio
Interface and connectivity ICs
Power management
ST25 NFC/RFID tags and readers
STM8 MCUs
Other: hardware
Other: software
Knowledge base
STM32 MCUs
STM32 MPUs
MEMS and sensors
Analog and audio
EMI filtering and signal conditioning
Interface and connectivity ICs
Power management
ST25 NFC/RFID tags and readers
Quality & reliability
Academy
About
Community guidelines
Feedback forum
Community blog
Developer news
ARaul.2
Associate II
since
2022-10-01
2023-06-14
User statistics
9
Posts
1
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About ARaul.2
Options
Report User
User Activity
Posts
Replies
i am trying to print on lcd via i2c and with stm32f103c6t6 but it is not working . there are no error in code also what should i do?
2022-10-27
these are project files of the project
can i upload code using stmcubeIDE to bluepill using uart module
2022-10-05
upload code using arduino ide for led blink and also for lcd,both time after uploading code its showing this Write to memory,Erasing memory Wrote address 0x0800fb38 (100.00%) Done. Starting execution at address 0x08000000... done. led notwork
2022-10-01
Re: i am trying to print on lcd via i2c and with stm32f103c6t6 but it is not working . there are no error in code also what should i do?
2022-10-28
this is set : #define SLAVE_ADDRESS_LCD 0x4Eaddress is 0x27 so it is perfect i guess
Re: i am trying to print on lcd via i2c and with stm32f103c6t6 but it is not working . there are no error in code also what should i do?
2022-10-28
lcd working perfectly when i run code via arduino ideand there are no errors also, can you please check out i2c files and code i have uploaded
Re: upload code using arduino ide for led blink and also for lcd,both time after uploading code its showing this Write to memory,Erasing memory Wrote address 0x0800fb38 (100.00%) Done. Starting execution at address 0x08000000... done. led notwork
2022-10-06
my problem is solvedactually the problem was with stmboard model ,i purchased stm32f103c8 but owner sent me stm32f103c6. i haven't noticed that , and also i was not thinking on that level that change in flash size will make this problem. Ty
Re: can i upload code using stmcubeIDE to bluepill using uart module
2022-10-05
so if i have cube ide folder with all programming files then that code can i upload using stm32CubeProgrammer via uart?
Re: upload code using arduino ide for led blink and also for lcd,both time after uploading code its showing this Write to memory,Erasing memory Wrote address 0x0800fb38 (100.00%) Done. Starting execution at address 0x08000000... done. led notwork
2022-10-05
yes!
View more