STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Single bank mode for STM32L471RxE devices

Hi EveryoneI'm having some trouble with the reference manuals description of single bank mode for the STM32L471RxE devices. In the attachments you can see that the page number for bank 2 always starts with 256, regardless of the flash size. What I co...

0693W00000aJa7GQAS.png 0693W00000aJaEzQAK.png
DWyde.1 by Associate II
  • 2418 Views
  • 4 replies
  • 0 kudos

Unwanted NMI interrupt of CSS peripheral of stm32G491CC

Good morning community,I am contacting you to ask for support regarding a EMC immunity problem I'm experiencing.My application uses an stm32g491cc MCU with an external 8 MHz ceramic resonator (HSE)What i observe is a reset of the microcontroller duri...

GIabi.1 by Associate II
  • 2198 Views
  • 0 replies
  • 0 kudos

STM32C0 Boot Programming

Hi, I am planning to use STM32C011F6 for a simple application and want to download application through UART1. How to use BOOT0 pin to program MCU for the first time. According to data sheet, UART1 pins PA9/PA10 needs remapping to function as UART. Al...

KGane.1 by Associate III
  • 1939 Views
  • 1 replies
  • 0 kudos

Resolved! [ STM32G070 ] STM32G070 input mode pin speed setting?

Dear Sir,​In STM32G070 series, the code shows the speed setting for GPIO output,If my GPIO is setting for input to receive external interrupt, does the speed setting also apply for GPIO input mode?Thanks/** @defgroup GPIO_speed GPIO speed * @brief ...

E-John by Associate III
  • 2488 Views
  • 2 replies
  • 1 kudos

SDIO API for H7

Sorry, I am new STM32 MCU :grinning_face_with_sweat: ​I want to bring up WIFI function with SDIO to connect Internet, but I cannot find any SDIO API in H7 like stm32f4xx_sdio.c.The link is where I can find the answer I want, but it only supports H747...

wG.1 by Associate II
  • 1954 Views
  • 1 replies
  • 0 kudos

STM32F407VGTX_FLASH.ld: No such file or directory error

Hi i wanted to try new extension but i get this error. The code is a basic blink its working on cubeide but when i try on vscode this happens.Thank you already[build] c:\st\stm32cubeide_1.10.1\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltoo...

HSarı.1 by Associate
  • 4267 Views
  • 4 replies
  • 0 kudos

Resolved! GPIO rise/fall time on Nucleo H7

I am prototyping an application on a Nucleo H7 board and I would like to use 50 MHz SPI master for performance reasons.At lower speeds (25 MHz, for example) I am able to generate a fairly clean SPI Mclk that passes requirements, however at 50 MHz I e...

Resolved! Change ADC clock in STM32H7

Hello, i'm using an STM32H7 but unfortunately for a known bug of the firmware package i'm not able to select the ADC prescaler. Uprading to a newer firmware package is not considered.At the moment i resolved applying a prescaler with the linehadc1.In...

0693W00000aJYovQAG.png
halbeeee by Associate II
  • 4890 Views
  • 4 replies
  • 0 kudos