Bug in HAL_ADCEx_Calibration_Start
The function using ADC_CALIBRATION_TIMEOUT. This timeout is defines as:/* Fixed timeout value for ADC calibration. */ /* Values defined to be higher than worst cases: low clock frequency, */ /* maximum presca...
The function using ADC_CALIBRATION_TIMEOUT. This timeout is defines as:/* Fixed timeout value for ADC calibration. */ /* Values defined to be higher than worst cases: low clock frequency, */ /* maximum presca...
I am able to receive data on the USART1 peripheral on the stm32h753-eval board using the character match and RXNE Interrupts. When I configure USART1 peripheral for FIFO mode, I set RXFTCFG to 1/8th in CR3, I enable the FIFOEN in CR1 and the RXFFIE i...
I am working with STM32H743, and I want to use Pin no. 89 as DAC output. Is there any register setting where I can change PA4 to PG4(89).I tried replacing PA4 to PG4 in a working example code, but the output still comes on PA4.
HI,I'm trying to create a Flash loader for ST-Link Utility or Cube-Programmer for STM32H750.I have successfully made the STM32F7 flash loaders, while with the STM32H7 I have the following problem:17:36:19 : Connected via SWD.17:36:19 : SWD Frequency ...
ADC:ADC1_Handler.Instance = ADC1; ADC1_Handler.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; //4·ÖƵ£¬ADCCLK=PER_CK/4=64/4=16MHZ ADC1_Handler.Init.Resolution = ADC_RESOLUTION_12B; //16λģʽ ADC1_Handler.Init.ScanCon...
Hey,I configured the stm32h743 to transfer data with sai2 and read the same data with sai1. Sai2 is in IT mode and works fine (checked it with a logic analyzer).The SAI2 is totally working in IT mode, but when I put it in DMA mode i only receive 0's....
Posted on August 17, 2017 at 13:48Hello, I tried the example 'FDCAN_Com_polling' on STM32H743I-EVAL, it worked like it should be.Then I separated the example code into TX part and RX part, made one of my STM32H743I-EVAL board as TX and another as...
I am looking for a STM32H753 evaluation board, this kind of board seems to be unvailable either on the ST site or the distributor site . Do you have some informations about this kind of evaluation board ? Where / when can I buy a STM32H753 evaluation...
There are multiple alternating functions for one peripherals. Why and what is the difference?
I want to use DMA on my stm32h7 board, but i can find which channel is used for what protocol ect.