User Activity

Good morning,I would like to use the "dynamicBitmapCreateExternal" function as my dynamic image is already present in flash in ARGB8888 format.I'm using GFX 4.16.1, compiling the compiler tells me Error [Pe020]: identifier "dynamicBitmapCreateExterna...
Hi,my application 800X480 consists of two modes: single and double.Single mode is full screen, made up of several screens, and it's ok.The second consists of the screen divided in half.Each half must be independent of the other, so it's like you have...
HI,I'm trying to create a Flash loader for ST-Link Utility or Cube-Programmer for STM32H750.I have successfully made the STM32F7 flash loaders, while with the STM32H7 I have the following problem:17:36:19 : Connected via SWD.17:36:19 : SWD Frequency ...
Hi, I'm trying to add the Printer class to a project with a USB host port.Is there any code available?The project was created with CUBE-MX and uses FreeRTOS.